User Activity

Dear all,I'm trying to run a TA application on STM32MP157C-DK2 board. Im using the STM32MPU Developer Package to build the TF-A and the OP-TEE.I've built the TF-A using the command below:make -f $PWD/../Makefile.sdk TF_A_DEVICETREE=stm32mp157c-dk2 TF...
Dear,I'm starting with OP-TEE on STM32MP15x line. I bring-up the board as described here and built the optee_example_hello_world as described here. However, I got the error code below:TEEC_Opensession failed with code 0xffff0008 origin 0x3Checking th...
Dear,Some images are not shown on STM32 MPU OP-TEE overview and STM32MP15 OP-TEE overview.Thanks!   
Dear,I'm trying to use the ETH with Zephyr RTOS 3.5.99. It was built the samples/net/dhcpv4_client sample, however, I tried to build others examples from samples/net/socket, such as echo and echo_client, but was impossible.I would appreciate it if an...
Hi everyone,How can I uninstall the STM32CubeProgrammer on Ubuntu? I check inside the folder and has an uninstaller.jar, but nothing happens. $ sudo java -jar uninstaller.jar   The uninstaller has put a log file: /tmp/izpack18013613561370631600.logA...
Kudos from