User Activity

We are currently experiencing a major issue with eMMC on our custom boards using STM32MP153CAC. Our boards are booting normally with 1 wire mode, but as soon as 8 wire/bit mode is enabled, it starts to bug out.Here is the description of the problem f...
When I'm working on configuring devicetree for a new board, adding new nodes and tweaking values, I often run into a un-bootable system. What I would like is that there is a bit more information of what goes wrong.Like now it just quits booting if so...
Hello we are using STM32mp153 for multiple products, and I'm considering buiding a generic TF-A bootloader with one device tree with all the clocks enabled for all the peripherals. I would like to do this in order to make it more generic across our p...
Problem: After configuring the OTP pins in word 3 to the following:- Primary boot source : SD-card- Secondary boot source : FMC NANDAnd flashing the FMC nand with TF-A `tfa-*-nand.stm32` in the first sector using `nandwrite -p /dev/mtd0 /mnt/boot/tf-...
Hi, Is there any way to give a more meaningful name to a serial port with the device tree, so that is shows up in the linux kernel?Right now, in a device tree, it is possible to choose an alias in the alias node. But they do show up as ttySTMx in th...
Kudos from
Kudos given to