Hello @Saranya_2003 ,
Could you please try these points:
Check that STLinkServer is installed or install it from this site.When you plug the board to the PC, It should enumerate as a STLink debug probe in device manager.Upgrade STLink firmware.Chec...
Hello @chris1seto and welcome to the community,
The problem is not reproduced with the latest version of CubeIDE. Could you specify which CubeIDE you are working with?
Thanks,
Rim.
Hello @slai-nick ,
This problem is not reproduced on Mac OS. So make sure that your code generation is correct and that you are using MacOS® 13 (Ventura) or MacOS® 14 (Sonoma) as this may affect some features in STM32CubeIDE.
Hello @Kier and welcome to the community,
I tried to reproduce the problem with a different variable type, but I couldn't reproduce it. Here is an example in the screenshot.
To further investigate the issue, could you share the variable type defin...