User Activity

Hi,I've just upgraded to version 4.16 of TouchGFX and noticed an issue with the new gauge widget.When I use a custom background image it does not get displayed correctly inside the application. It's displayed somewhat "zoomed in". I've attached a scr...
I am currently seeing an assert_param failure within the HAL_ADC_Init() method in stm32h7xx_hal_adc.c file.Specifically the following assertion is failing:assert_param(IS_ADC_RIGHT_BIT_SHIFT(hadc->Init.Oversampling.RightBitShift));The value being pas...
CubeMX Version : 6.0.1.202008101643 com.st.stm32cube.common.feature.mxDevice: STM32H743I believe there may be an issue when setting the VREFBUF output voltage in CubeMX. The definitions for VREFOUT in CubeMX are inconsistent with the definitions give...
Hi,I'm having an problem whereby I believe the temperature readings from an HTS221 device are incorrect. They seems to be around 5degC too high compared to reference temp. I'm using a Nest thermostat as the reference, and while this may not be calibr...
Kudos from
Kudos given to