User Activity

Hello,I'm facing a bizarre issue with USART2 in STM32H7 chip.My H7 is connected to 8 F072 chips via UART. Communication with each chip uses a dedicated UART from 1 to 8.All the data exchanges in both RX and TX work fine during normal operativity of m...
Hello,I'm in Cube MX and trying to activate the LSE option of my NUCLEO-H723ZG but the option is not available. I see many others which are notavailable.Why? I see that the external low frequency oscillator is correctly installed into the board...Che...
Hello,I'm trying to have a list of MCU with TSC (touch sensing) and Timer comparator with quadrature encoding features but it looks like these are not listed in MCU finder or CubeMX.Is there a way to have this filtering?Thanks in advance,Filippo
Hello,I am testing a STM32C0 MCU to see if it might be good for a project I'm working on attracted by the price point, but I have to say that I have some unexpected problem.Among several the most relevant is multichannel DMA based ADC conversion that...
Hello,After prototyping with a Nucleo H7 board, I'm setting now up a custom board with a STM32H723ZGT6 MCU (the same MCU present on the Nucleo).I connected my USB Dongle ST-Link V2 via SWD to program the MCU and after having struggled a bit, I have f...
Kudos from
Kudos given to