Hello sbhowmick94,
The default state of the nBOOT1 bit for BOOT configuration is set to 1, it's written in the RM0351 :
https://www.st.com/resource/en/reference_manual/rm0351-stm32l47xxx-stm32l48xxx-stm32l49xxx-and-stm32l4axxx-advanced-armbased-32bit...
Hi Inkong,
Can you try downloading on another browser? Or you can try to log out and download as guest also to see if it solves the issue.
Regards,Stassen
Hello Nevase123,
All the examples of the H7 are found in the H7cube found on st.com including the STM32H735-DK.https://www.st.com/en/embedded-software/stm32cubeh7.html
Regards,Stassen
Hello Marekvecera,
You can also have a look at AN5105. There are 2 examples working in pooling mode for slider and button based on DISCO-F072B&L0538. See chapters 7.2 and 7.3.
As TSC peripheral is the same in L0, F0, F3, L4 software and design will b...