cancel
Showing results for 
Search instead for 
Did you mean: 

Nucleo-G474RE board - STM32G474RE - ADC -> EOC flag is not set.

mdudhat
Associate II

Hi all,

The project is under Nucleo-G474RE board using STM32CubeIDE.

I am trying to use ADC1 in continuous conversion mode but unfortunately the code hangs at while((ADC1->ISR & ISR_EOC)!= 1){} loop.

as i am checking the conversion to be finished and then checking the conversion result on DR register. Your suggestions/advices are highely appreciated. Thank you.

2 REPLIES 2
Stassen.C
ST Employee

Hello mdudhat,

We will need a bit more information on the setup of your project to be able to help you, is everything setup correctly?

Regards,
Stassen

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Hello Stassen.C,

thanks for the reply. actuallly i havent used any HAL/LL based drivers, based on STM32CubeMx but its just from scratch like using frimware package (stm32g4xx.h) and required registers bit setting for ADC.

For the registers:

ADC1->SQR1, ADC1->CR, ADC1->CFGR etc.  are used to set sequence start, sequence length,enableing module, start conversion and finally i read the register DR for the result. I am reading the result in polling mode.

Thank you.