Skip to main content
darla14
Associate III
January 11, 2023
Question

Error: hci_le_set_scan_response_data [ff] in STM32CubeFunctionPack (en-fp-sns-motionenv1)

  • January 11, 2023
  • 0 replies
  • 1298 views

Hello,

I am using F401RE Nucleo + X-NUCLEO-BNRG2A1 + IKS01A2 and FunctionPack 4.2.1 .

After dragging the _BL_v4.2.0 bin to the nucleo on resetting the board i am getting this :

Error: hci_le_set_scan_response_data [ff]

while on another board it is giving : aci_gap_update_adv_data OK

What is the cause of this on the first nucleo board?

Do i need to flash the module again?

Regards,

D

This topic has been closed for replies.