2012-02-15 7:19 AM
Hello,
I want to use a a advanced control timer (TIM8) of my STM32F103ZG (on STM3210E-EVAL) for motor control. I have problems generating the PWM signal at the right time. I initialize the timer the same way as in the 6-step example out of the std. peripherals lib examples, i.e.: TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_Timing; Later I try to start the PWM output mode with: TIM_SelectOCxM(TIM8, TIM_Channel_1, TIM_OCMode_PWM1); TIM_CCxCmd(TIM8, TIM_Channel_1, TIM_CCx_Enable); This has no effect. When I use TIM_OCInitStructure.TIM_OCMode = TIM_OCMode_PWM1; instead in the init phase, then PWM output works. I use an oscilloscope for verification. Thanks. best regards, sebastian2012-02-16 2:24 AM
Hi Sebastian, I had the same problem. Solution is that you should be also change to PORT and PIN.
You can find right port and pins the next Document ID 15818 Rev 8 table 7. If you want to use timer 8, using port C and pin numbers 6(channel 1),7(channel 2),8(channnel 3) and 9(channel 4). And remember that those pins are also connected to timer 3. BR: Pentti2012-02-16 4:02 AM
Hi,
I don't understand exactly what you mean. The appropriate GPIOs are already configured correctly for alternate function, e.g. GPIO_InitStructure.GPIO_Pin = GPIO_Pin_0 | GPIO_Pin_1; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(GPIOB, &GPIO_InitStructure); What else do have to do with them? In the 6-step commutation example delivered with the std peripheral lib, I cant find more information, too. regards, sebastian2012-02-16 10:00 PM
Hi Sebastian, if you want to use timer 8 the you have to use Port C. Channel 1 is connected to port C pin 6, channel 2-> PC7, channel 3-> PC8 and channel 4-> PC9.