Hello,Since STM32CubeIDE V1.11.0, there is an issue in linker file template, see STM32WB55RGVX_FLASH.ld file. In this file, there is an extra dot for MB_MEM2 section initialization, see this part: .MB_MEM2 :
{
_sMB_MEM2 = . ;
*(.MB_MEM2) ; ...
The new STM32WBA series comes to complete the STM32 Wireless MCUs portfolio.
The STM32WBA series is brings designers the performance, efficiency, and security required for Bluetooth® Low Energy 5.3-enabled applications.
Certified for Bluetooth® Low...
Hello, A corner case has been recently identified with FUS v1.2.0. It is not possible to upgrade back-to-back a wireless firmware with a new version that is exactly one sector bigger than the installed version. This limitation applies only when the r...
Hello,
You can refer to the following wiki page for more information regarding Bluetooth LE Audio architecture and integration on STM32WBA, on section 3.1 "Configuration of the audio profiles of the Generic Audio Framework".
The error code 0x07 means...
Hello,
It's a know issue on STM32WBA5x revision A describe in stm32wba5x device errata sheet (ES0592), see part "2.2.3 SYSCLK may not reach the PLL1 frequency when step switch is enabled". The workaround is implemented in HAL under the STM32WBAXX_SI_...
Hello,
If you perform some action with STM32CubeProgrammer to run the FUS on CPU2 like "Start FUS", "Read FUS version", "Delete wireless stack", the FUS will run on CPU2, that's why you see FUS_FW_RUNNING in the ready event. For example, after an upg...
Hello,
To work with Matter over Thread, you should use the X-CUBE-MATTER available on ST website. To have more details on each binary you can refer to the release notes, for Matter you should use the binary available in the X-CUBE-MATTER:
stm32wb5x_...