Posted on May 30, 2006 at 05:52Kindly let me know whether the ouput compare feature in ST7FL35 is for generating an interrupt alone or for directing it to the output pin and generating pulse with it. Thanks, Suganya
Posted on May 02, 2006 at 04:12Micro Used: ST7FL35 Tool Used: DVP3 Compiler: Cosmic Not able to configure PA5 (HS)/ATPWM3/ICCDATA and PA6/MCO/ICCCLK/BREAK. If written it causes a reset while ICD.It works fine with the default configuration of PADDR ...
Posted on May 02, 2006 at 03:51Micro Used: St7FL35 Tool Used: DVP3 Issue: Micro does not start as a stand alone device once it is removed from the debugger. I read back the contents of the ROM and option byte info after the debugger is being used. A...
Posted on April 07, 2006 at 08:32Controller used: ST7FL35 Compiler: Cosmic Tool: DVP3 SW: STVP7 When i execute my application in the ICD mode, i encounter a reset when i try to configure a pin(other than ICCCLK(PORT A bit6) and ICCDATA(PORT A bit5))...
Posted on April 04, 2006 at 02:10Thanks WoRo, It worked with out the error, but the return value from the RC calibration value location is always 0xFF. Is this the calibration value stored for a 1 Mhz clock to be generated? Regards, Suganya