cancel
Showing results for 
Search instead for 
Did you mean: 

Port Configuration

sjayapal
Associate II
Posted on May 15, 2006 at 19:09

Port Configuration

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
sjayapal
Associate II
Posted on May 02, 2006 at 04:12

Micro Used: ST7FL35

Tool Used: DVP3

Compiler: Cosmic

Not able to configure PA5 (HS)/ATPWM3/ICCDATA and PA6/MCO/ICCCLK/BREAK. If written it causes a reset while ICD.It works fine with the default configuration of PADDR = 0x00 and PAOR = 0x40. If i change the configuration to PADDR = 0x40(or 0x60) and PAOR = 0x00. When in ICD mode it resets. I would like to configure PA5 has output pin in my application. When in ICD mode i am taking care as to not use this pin in my application.As i understand from the data sheets to just configure it has output i feel it should not cause a problem.

Kindly let me know as to what is going wrong?

Regards,

Suganya

info45
Associate II
Posted on May 15, 2006 at 19:09

Hy Suganya,

humm....from data sheet You can set Pa5 and Pa6 in otuput mode, but follow the I/O port sequence configuration! PADDR 0x40 and Paor 0x00 means open drain configuration, then need a pullup resistor!

For your throuble, are You sure that your HW don't produce strangerous effects?

I think that is better isolate this pins from your HW and follow step by step ( register load) the micro situation.

Other, I see that this pinst are connect in input to external interrupt logic...

By