Posted on June 29, 2009 at 14:43I have been developing an application on the ST72F324LK6T6 with DVP3. During emulation all is well. When I solder chip to app board and try to ICP program (with STVP ) I get an error message ''PROBLEM DOWNLOADING MONI...
Posted on June 25, 2008 at 14:34I'm using the 72F324B in an application and trying to use Active Halt mode. Most of the time the application enters and exits active halt mode correctly but randomly the cpu resets. I can see from my trace that the pr...
Posted on February 08, 2008 at 17:50Hi luca Thanks for you response. I think you have misinterpreted my post. The code is optimised down to a single jrpl instruction ! There is no instruction preceding it to set the flags for the conditional jump. S...
Posted on February 06, 2008 at 07:52I posted on here a while ago about a problem with the Cosmic compiler optimiser V4.5d. I have now tracked this down. Current version is V4.5.5. Changes between V4.5d and V4.4.5 are not relevant, so this bug is sti...
Posted on November 05, 2007 at 08:26How do I enable / disable optimiser on file basis ? It is difficult to debug with optimisation on, there doesn't appear to be good debug info generated for the emulator.