cancel
Showing results for 
Search instead for 
Did you mean: 

Comic Compiler optimisation

patm4
Associate II
Posted on November 05, 2007 at 09:39

Comic Compiler optimisation

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
patm4
Associate II
Posted on November 02, 2007 at 12:15

I have been developing an application under ST7VD/Cosmic C/DVP3

The application runs fine on the debugger with DISABLED FOR DEBUGGING build ( Optimisation OFF )

If I build a RELEASE version with the Optimisation DISABLED FOR DEBUGGING and run on the target then all is again OK.

If I build a RELEASE version with DEFAULT optimisation and run on the target the application behaves differently ( errantly ).

I also tried setting the optimisation to custom and messing about with the options but no combination makes the target app. run correctly.

I assume this is an optimiser problem, but I can't see how to track it down. Are there an compiler switches/directives I can use on a per file or per function basis to turn on/off the optimisation.

luca239955_st
Associate III
Posted on November 05, 2007 at 06:33

Hello,

as you describe it, it looks like an optimization error indeed.

Note first that we (Cosmic) recommend to work with optimizations ON since the very beginning of the project.

Here are some suggestions:

1) make sure you are using the latest version of the compiler

2) the best way to find the ''optimization problem'' (that could be in the toolchain or in the application) is to debug the application

3) if you can't use point 2), you can try to enable optimizations only file by file: if every file contains only a few functions, this will give you a first direction for your investigation.

Regards,

Luca (Cosmic)

patm4
Associate II
Posted on November 05, 2007 at 08:26

How do I enable / disable optimiser on file basis ?

It is difficult to debug with optimisation on, there doesn't appear to be good debug info generated for the emulator.

luca239955_st
Associate III
Posted on November 05, 2007 at 09:39

>> How do I enable / disable optimiser on file basis ?

I guess you use STVD7, which is not a Cosmic product, so I don't know the answer, but I think it should not be too difficult to find out.

If you use the command line, just remove the ''-no'' for the file(s) where you want the optimiser to be active.

>> It is difficult to debug with optimisation on...

that's surprising, please provide an example, if you have time.

Regards,

Luca