2009-06-29 5:43 AM
Problem ICP programming ST72F324L device with STVP
2009-06-29 5:43 AM
I have been developing an application on the ST72F324LK6T6 with DVP3.
During emulation all is well. When I solder chip to app board and try to ICP program (with STVP ) I get an error message ''PROBLEM DOWNLOADING MONITOR'' I have programmed many devices with this setup and not had problem, but this is the first time on the 3v parts. I have done the following:- 1) Checked the ICC schematic against the datasheet. 2) Removed target crystal, connected ICCOSC to OSC1 and connected OSC2 to GND. The ICCOSC signal has been checked with a scope for the presence of a clock. 3) Checked DVP settings ICP-OPT Disable and 3V app. supply switch setting. I have read a little about the ICC protocol and have confirmed the pulses on ICCDATA. One thing I did note was that the VOH levels on the ICCDATA and ICCCLK are a little marginal ( 2.4-2.5v ). I tried pullup resistors on the app board on these lines but it made no difference. The RESET and ISPSEL lines also seem ok. Any suggestions ? Are there any firmware updates for DVP3 ?2010-07-28 10:31 PM
.ExternalClass23B559A9A8F945A4B8214D961234490B p.MsoNormal, .ExternalClass23B559A9A8F945A4B8214D961234490B li.MsoNormal, .ExternalClass23B559A9A8F945A4B8214D961234490B div.MsoNormal {margin:0in;margin-bottom:.0001pt;font-size:11.0pt;font-family:'Calibri','sans-serif';} .ExternalClass23B559A9A8F945A4B8214D961234490B .MsoChpDefault {font-size:10.0pt;} @page Section1 {size:8.5in 11.0in;margin:1.0in 1.0in 1.0in 1.0in;} .ExternalClass23B559A9A8F945A4B8214D961234490B div.Section1 {page:Section1;} Did You Get Solution for this.
Kindly Share if You have.