EZHON.1
ST Employee
since
2021-10-08
2024-06-27
User statistics
14
Posts
0
Solutions
0
Kudos given
3
Kudos received
View all badges
STMicroelectronics Community
About EZHON.1
Options
Report User
User Activity
Posts
Replies
No posts to display.
Re: STM32C0116-DK CN1/CN5 extension connectors?
2024-06-26
CN5 is inherited by Morpho connectors CN10. for CN1 connection, we can use flying wires without other choice for the small size board.
Re: Connecting SD CARD to STM32H743 without level translator
2023-12-13
STM32H743I-EVAL supports SDIO3.0 interface microSD™ card while STM32H747I-DISCO supports SDIO2.0 interfacemicroSD™ card. They are different SDcard specifications.
Re: Connecting SD CARD to STM32H743 without level translator
2023-12-13
when inserts SD card, there is a voltage drop for 3.3V rail. it should be better to add a dedicated LDO for SD card.
Re: STM32 Discovery and 5V logic
2023-10-26
Arduino connectors for STM32 GPIO is 3.3V, not 5V. if 5V for LEDs, it's better to add level shifter for them.
Re: STM32G474 USB-TYPE-C
2023-10-23
You should check your board with Type-C connector or not?
View more
Kudos from
User
Count
Mosi
2
waclawek.jan
1
View all