User Activity

Posted on September 06, 2016 at 08:13Hello,I want to interface a SD card with stm32f303. Please help me how to interface sd card with microcontroller. Also I want to read the data on my laptop, do I need a file system because windows can read in FAT...
Posted on September 02, 2016 at 09:10Hello,I am using gsm module to transmit a message using USART of stm32f303. I have used following commands for gsmAT+CMGF=1AT+CMGS=''+923046761738''at the end it requires CTRL+Z to send the message but usart is n...
Posted on June 30, 2016 at 07:02Hello!I am using AM26LV31I driver for RS422. The power dissipation is written in datasheet as:Ultra-Low Power Dissipation� dc, 0.3 mW Max� 32 MHz All Channels (No Load), 385 mW TypCan anyone please tell me what is thi...
Posted on June 27, 2016 at 19:40Hello I am developing a evaluation board for STM32F427. I am connecting an external **RTC** IC (DS3231). Do i need to connect an other external oscillator for processor? Because in STM32F407 discovery board they have ...
Posted on June 23, 2016 at 18:38I am working on Stm32f427. I want to interface EEPROM with this microcontroler for external booting. The external booting options mentioned in referance manual are from system memory and SRAM. Please tell me how to in...