2019-04-11 2:51 AM
I downloaded and installed the COSMIC stm8 free compiler (http://cosmicsoftware.com/download_stm8_free.php).
I requested and received a license.
I copied the license file to the appropriate folder.
However, the compiler does not start.
It does not start from ST Visual Develop.
I tried to run it on the command line, from the folder in which it is located (D:\Program Files\COSMIC\FSE_Compilers\CXSTM8).
I see error: "D:\Program Files\COSMIC\FSE_Compilers\CXSTM8\cxstm8.exe not a valid Win32 application"
I use Windows XP SP3.
I tried 3 times reinstall compiler. And i got same error.
2019-04-11 3:28 AM
Cosmic has it's own user forum, and promises installation support. Have you tried it there ?
Not much seasoned STM8/Cosmic users present here.
2019-04-11 9:35 AM
No, I have not tried it yet.
The file Readme.txt says "If you have any question, please post them on: https://my.st.com/public/STe2ecommunities/mcu/default.aspx or send e-mail to support.stm8.free@cosmic.fr".
And so I wrote here.
Do not tell me a link to the COSMIC forum?
2019-04-20 2:27 PM
I am looking at my Project settings and it looks like it automatically set the path to C:\Program Files(x86)\COSMIC\FSE_Compilers\CXSTM8 - try to install everything with default paths.
You can also try to ensure that in your project settings the path is correct.
2019-04-21 11:55 PM
Thanks for the help.
I wrote to the support team and they told me that their compiler no longer supports running on Windows XP.
Nothing can be done about it.
The topic is closed.