STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

An online debugger for stm8s MCUs

Hey guys.I need to watch my variables online.On stm32 there was stm studio which I could watch them.I use IAR as my compiler but for watching a variable I have to pause the debugger to see its value.Whats your offer?

Chip Not Responding Error [stm8s005k6t6c]

Hi All,We use stm8s005k6t6c IC in one of the circuits. We programmed the IC using IAR embedded workbench IDE. We attached the circuit diagram herewith for your reference. But we couldn't get any success of programming it since we receive an error say...

0690X000006C1EVQA0.png

STM8L1528 ADC, DMA, TImer not working together.

Hi there,I am developing code for STM8L1528 EVAL board. My goal is to configure adc with dma(peripheral to memory) where adc should collect data for certain period, for example, 2 seconds.So I configured adc and dma according to examples codes given....

Gopal by Associate
  • 838 Views
  • 2 replies
  • 0 kudos

External Interrupt in PORTB (Multiple pin)

I configure the portB 4,5,6,7 as external interrupt pins. the program is working well if any interrupt occurs in portb 4,5,6,7 the execution send to irq. how to find which pin irq is occured in portbplease give the solution to my problem

RKuma.7 by Associate
  • 737 Views
  • 2 replies
  • 0 kudos

Option bytes complementary error with manual write

Hello.I'm trying to set Option bytes on STM8s005k6 from main code, but still I'm getting error in complementary bytes (when I try to rad out it back in STVP) and MCU hangs.I'm using SDCC compiler with this code: // Set option bytes because of buzzer ...