2013-01-04 7:43 AM
As the software is a free software, there is no direct support. Support is
done via the discussion forum on
/public/STe2ecommunities/mcu/default.aspx
That's isnt dumb and headless ?
Sorry.
2013-01-05 1:35 AM
Yes it is dumb :( It is why other MCU families are more interesting for small developers.
ST should really have released a proper free toolchain for the STM8 line instead of relying on other parties.2013-01-05 11:55 PM
2013-03-04 9:31 AM
This is not a dumb request. The IDE should provide a ''dashboard'' with flash usage, RAM usage, and other information, like competing IDEs do.