2018-04-19 05:52 AM
Hello, i have an STM8L1526 board, and i don't success to connect with my computer. I use ST visual develop but it doesn't work. I want to use the STM8L152C6 to drive some of led on extern electronic plateform ( prototype). thks for your help
2018-04-19 08:45 AM
I do not see how to replace the built-in default programs, so that I can implement my own
2018-04-19 12:09 PM
'
it doesn't work'
I guess you make it work then?
The amount of help you get is full dependent on the quality of information you provide.
2018-04-20 02:56 AM
When i implement my code, this software bugs and leaves
2018-04-20 03:17 AM
2018-04-20 07:18 AM
Hello,
This issue is already confirmed, see the post above, there is a workaround.
https://community.st.com/0D50X00009XkWxBSAV
Rgds,
Laurent