cancel
Showing results for 
Search instead for 
Did you mean: 

STM8L1526-eval board problem

jeremy pouteau
Associate II
Posted on April 19, 2018 at 14:52

Hello, i have an STM8L1526 board, and i don't success to connect with my computer. I use ST visual develop but it doesn't work. I want to use the STM8L152C6 to drive some of led on extern electronic plateform ( prototype). thks for your help

5 REPLIES 5
jeremy pouteau
Associate II
Posted on April 19, 2018 at 17:45

I do not see how to replace the built-in default programs, so that I can implement my own

henry.dick
Senior II
Posted on April 19, 2018 at 21:09

'

it doesn't work'

I guess you make it work then?

The amount of help you get is full dependent on the quality of information you provide. 

Posted on April 20, 2018 at 09:56

When i implement my code, this software bugs and leaves

Posted on April 20, 2018 at 10:17

0690X00000604abQAA.jpg
Posted on April 20, 2018 at 14:18

Hello,

This issue is already confirmed, see the post above, there is a workaround.

https://community.st.com/0D50X00009XkWxBSAV

Rgds,

Laurent