cancel
Showing results for 
Search instead for 
Did you mean: 

STM8AL3189TCX NRST pin is asserted what happens to MCU output

Mlokesh
Associate

Hello All,

we are using STM8AL3189TCX MCU in our design to control the system.

A WDT signal "MCU_NRST" is connected to NRST(PIN-2, NRST/PA1) pin in microcontroller with a Pull up to 3V3.

What will happen to MCU IC when the below reset condition occur: 

Condition:- If WDI pulse from HOST MCU fails this condition (Lower Boundary (tWDLmin) = 19.1ms-25.6ms & Upper Boundery (tWDUmax) = 46.8-63.3ms)

HW Action:- Supervisor will asserted low to reset, HOST MCU to turn off the system

Is the hardware action mentioned is correct?

Watch dog Part#- TPS3850H33QDRCRQ1

0 REPLIES 0