2018-01-04 4:40 AM
Hello community,
i try to programm an code for my experimentation and i have a problem .. my code should change the duty cycle ie. the value of CCR2_V if the value of Convertion_Value_Current exceeds or is below a specific value .. as a result i want to see on the oscilloscope a changing pwm but it is still with the same duty cycle as defined in the main (CCR2_V=27)
the idea was to increment or decrement the value of the register, but it does not working. Have you any ideas where the problem can be?
Thanks
BG
&sharpinclude <stm8s.h>
&sharpinclude <stm8s_eval_lcd.h>&sharpinclude <stdio.h>uint8_t StrName[16]={0};uint16_t Conversion_Value = 0;float Stufe = 0.00488;float Nominal_Min = 3.500;float Nominal_Max = 4.500;float Conversion_Value_Current = 0;uint16_t CCR2_Val = 27 ;uint8_t a = 50;// Parametrisierung des PI Reglers !!!! MUSS NOCH IN MATLAB BESTIMMT WERDEN !!!! //float kp = 0.001;float tn = 0.04;int main(void){
// Systemtakt
CLK_HSIPrescalerConfig(CLK_PRESCALER_HSIDIV1); // Erzeuge PWM TIM3_DeInit(); TIM3_TimeBaseInit(TIM3_PRESCALER_1, 45); TIM3_OC2Init(TIM3_OCMODE_PWM1, TIM3_OUTPUTSTATE_ENABLE,CCR2_Val, TIM3_OCPOLARITY_HIGH); TIM3_ARRPreloadConfig(ENABLE); TIM3_OC2PreloadConfig(ENABLE); TIM3_Cmd(ENABLE);// Initialisiere ADC und LCD STM8S_EVAL_LCD_Init(); GPIO_DeInit(GPIOB); ADC2_DeInit(); GPIO_Init(GPIOB, GPIO_PIN_2, GPIO_MODE_IN_PU_NO_IT); ADC2_Init(ADC2_CONVERSIONMODE_CONTINUOUS, ADC2_CHANNEL_2, ADC2_PRESSEL_FCPU_D4, ADC2_EXTTRIG_TIM, DISABLE , ADC2_ALIGN_RIGHT, ADC2_SCHMITTTRIG_CHANNEL9, DISABLE); ADC2_Cmd(ENABLE); LCD_Clear(); LCD_BacklightCmd(ENABLE); ADC2_StartConversion();
LCD_SetCursorPos(LCD_LINE1, 0);
LCD_Print('Convers.Value.:'); LCD_Print(' '); while(1) { while(!ADC2_GetFlagStatus()){} Conversion_Value = ADC2_GetConversionValue(); Conversion_Value_Current = Conversion_Value*Stufe; //Regelung der Duty Cycle f�r einen erw�nschten Ausgangsstrom if(Conversion_Value_Current > Nominal_Max) { CCR2_Val--; } else if (Conversion_Value_Current < Nominal_Min) { CCR2_Val++; } TIM3_OC2Init(TIM3_OCMODE_PWM1, TIM3_OUTPUTSTATE_ENABLE,CCR2_Val, TIM3_OCPOLARITY_HIGH); sprintf((char*)StrName, '%.3f ', (Conversion_Value*Stufe)); LCD_SetCursorPos(LCD_LINE2, 0); LCD_Print(StrName); ADC2_ClearFlag(); } } #stm8/128 #pwm-stm8 #stm82018-01-04 5:51 AM
Would probably avoid preloading the CCRx, but rather let the new value latch at the update event.
2018-01-04 7:25 AM
Hello Clive One, thanks a lot for your fast reply and support.
But when I do not preload the CCR2, then i do not have the waveform .. slow on the uptake, sorry i do not quire get it
How the buffering the new value would be look like in the code?