2011-09-18 10:13 AM
I use STM8 Assembler.
Code: ...... CLOCK EQU 16000 TIME EQU CLOCK/1000 .... compile error Error 67: Improper Character(s) '/1000' Why? I find :) TIME EQU {CLOCK/1000} Works without errors2011-10-06 1:49 AM
Hi.
At increase in the size of a code the program does not work. Has started a debugger - the instruction call xxxx has the size of 3 bytes - CD xx xx (where xx xx the absolute address of procedure), though in PM0044-STM8 - call xxxx has the size of 4 bytes - 72CD xx xx ? At size increase the absolute address xx xx varies on not the correct My code: call MyProc ........; If here to add instructions, the xx xx - address is generated incorrectly
........ MyProc.w ........ ret2011-10-06 4:21 AM
Hello Pavel.
What the debugger shows is right. The assembler translates CALL MyProc to CD xx xx, where $xxxx is the address of MyProc. 72 CD xx xx is instead the translation of CALL [MyProc.w] where MyProc ''points'' to the code to be called. If your code doesn't work when its size grows, you have to execute it step by step until the error happens. After you spotted the place, compare your code with the disassembled one and you'll find the error reason. BR EtaPhi2011-10-06 5:05 AM
T
hanks
EtaPhi Similar the error consists wrong generation of the address for СALL instructions ... This error is described here [DEAD LINK /public/STe2ecommunities/mcu/Lists/stm81/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/stm81/Problems with JP and CALL instructions&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580001E3853D9DB932A46A3FE4CD15CAB46FB&TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/stm81/AllItems.aspx¤tviews=52]- Problems with JP and CALL instructions