‎2018-05-12 6:28 AM
Hi everyone. I am working with STDV development tool. When I want to build the program, the message 'the executable can not be found' appear. How can I modify the settings to solve this problem??
‎2018-05-14 12:26 AM
Hello,
Which C compiler you would like to use in your project?
May I ask you to pass me a screenshot from your settings of the project, please (please click left button on mouse over the project name and select Settings, then please select General tab)?
First thing which I would check is whether the toolset paths are set correctly (compiler, linker).
Thank you in advance,
Best Regards,
Artur
‎2025-03-10 7:25 AM
STVP=St visual programmer, STVD=St visual Develop, NOW STDV=??? i want to debug stm8 series MCu. what software i need?
‎2025-03-15 5:42 AM
Use STVD. STVD already have STVP. You should start with a development board and it already have ST-Link.
‎2025-03-15 9:31 AM
COSMIC compiler working fine. compiled wwithout error, then build no issue, then burn by stVP help of cloned stlink-v2 usb type ,no issue programe run at MCU. but when i go to debug in STVD it says communication error 30006. have a look screen shot. if stlink cloned i am using swim pin working when programe uploading, but debuging mode not working. taken screen shot from logic analyzer, if you would like to deep dive.
‎2025-03-15 9:33 AM
RST and SWIM pin timing diagram when debug mode.
‎2025-03-15 9:38 AM
if yiu are using cosmic compiler then set project specifif toolset path(you will find project->setting->project setting C:\Programe Files(x86)\COSMIC\FSE_Compilers\CXSTM8
‎2025-03-15 9:43 AM
Compiler COSMIC. please confirm that if i use stm32 based dev board then inbuilt stlink v2 is usefull to dubug core board of stm8S or STM8A series ?
‎2025-03-16 1:40 AM
You should use a development board as STM8S-DISCOVERY or use ST-LINK/V2 in-circuit debugger/programmer for STM8 and STM32.