2023-08-29 05:58 AM
Dear ST-Team,
I am working on a STM8 MCU with the STVD.
I want to compile my project in the Microsoft cmd line with a pipeline such as . cmd.exe /c "C:\Program Files (x86)\STMicroelectronics\st_toolset\stvd\stvdebug.exe"
I haven't found any information in the Documentation. Furthermore, there are no help options such as -h, --h, -help and --help in this program.
Are there some documents I can use to write the correct commands to compile the code with the STVD successfully?
Many thanks in advance
Best Regards
Stefan
2023-08-29 10:24 AM
STVD doesn't include the compiler. Read this: Developing and debugging your STM8S-DISCOVERY application code. The recommended compiler is from COSMIC.
2023-08-30 12:00 AM
Thanks for your quick response.
I am using the Cosmic compiler already.
I want to use the CMD line. Is there a Possibillity that I can use the CMD with a pipeline for compiling.
I have found another documentation from an other manufacturer: Create and Build Projects Using Command Line (ti.com).
Is this also with STDV possible? e.g.: cmd.exe /c "C:\Program Files (x86)\STMicroelectronics\st_toolset\stvd\stvdebug.exe <workspace> <file location> <build Parameters>"
2023-08-30 05:39 AM
I don't know if you can compile from command line using STVD. Probably no. But you can ignore STVD and use the compiler and the linker directly. See Cosmic manual.