cancel
Showing results for 
Search instead for 
Did you mean: 

radiation from mobile phones -> auto reset?

master
Associate II
Posted on April 19, 2011 at 10:42

Hello,

I have just finished my project, but unfortunately I have a problem at the end. ;) My Stm8s Discovery is in a plastic box together with a cell phone. When the cell phone get switched on, the

microcontroller

resets itself. Is this normal? Has anybody of you a glue to solve this problem? Maybe without extra shielding? When I put the mobile more than 15cm away from the

microcontroller

, it works... but the box is small...

Thanks in advance

Klaus

#shielding-cell-phone-reset
1 REPLY 1
brazov22
Associate II
Posted on April 19, 2011 at 15:46

put the discovery board inside a aluminium paper :)