cancel
Showing results for 
Search instead for 
Did you mean: 

BLUENRG-M2SA: Slave Device connected to two different Masters

ilias
Associate II

Hello, I am in the development of a project that we need our BLUENRG-M2SA device to be configured as a Slave device (PERIPEHRAL role) and connected to two different Masters devices (two different Mobile Phones).

My questions are:

  1. Is this supported by the BLUENRG-M2SA because I couldn't find something clear on the documentation.
  2. If yes, Is there any example that I could use for that?
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
ilias
Associate II

Hi,

I forgot to mention that the slave device should be connected to the two Masters devices simultaneously.