cancel
Showing results for 
Search instead for 
Did you mean: 

PWM capture with TIM1?

georg23
Associate II
Posted on March 14, 2010 at 23:01

PWM capture with TIM1?

12 REPLIES 12
georg23
Associate II
Posted on May 17, 2011 at 15:07

hi,

thanks for the fast response! I have now copied the very procedure described in the STM8 reference manual - still without success. Guess I have to contact technical support..

Regards, Georg

lowpowermcu
Associate II
Posted on May 17, 2011 at 15:07

Hi,

I remember that I used this config and it worked fine. Perhaps you missed this step

''Select the valid trigger input: write the TS bits to ‘101’ in the TIM1_SMCR register (TI1FP1 selected).''

It is indicated in the reference manual !

regards,

mcu fan

lowpowermcu
Associate II
Posted on May 17, 2011 at 15:07

Hi georg,

you can send me your code perhaps I can help you.

Mit besten Grüßen,

low power fan

georg23
Associate II
Posted on May 17, 2011 at 15:07

hi,

thanks a lot in advance! Of course I can provide you with a demo project for the Discovery Board (see attachments to this post). For your help and effort thanks a lot in advance!

Regards,

Georg

lowpowermcu
Associate II
Posted on May 17, 2011 at 15:07

Hi georg,

After a first look. I suggest to change

    while (!TIM1_SR1_UIF);

by

    while (!TIM1_SR1_CC1IF);

because it is at capture event the counter value will be loaded in capture register.

Hope this helps.

Tell if it is OK

Mit besten grüssen,

MCU Lüfter

georg23
Associate II
Posted on May 17, 2011 at 15:07

hi Lüfter,

funny discussing in english when both our native language most likely is german...? Anyway, I've tried your proposal but I still get a funny result (see attachment). The columns are (from left to right): input frequency and duty cycle (both asserted using an oscilloscope), TIM1_CC1 and TIM1_CC2 capture values, and the calculated frequency (24MHz/2/CC11) and duty cycle (CC2/CC1). 

To me this seems like CC1 & CC2 do capture the edges, but for some reason the timer doesn't start correctly...? This is also supported by the observation that the 1st measurement is only slightly off (starts immediately after start of PWM generation), whereas all the other measurements are more off (+ some ms delay). Any idea???  And again, thanks in advance for any help!

Regards, Georg

lowpowermcu
Associate II
Posted on May 17, 2011 at 15:07

Hi georg,

You put 1KHz and you find in CCR1 12000. Das kommt nicht !

If your timer is clocked by 16 MHz so you should have 16000 in CCR1 register +/- error. What is your clock divider, timer clock 16 MHz, 8MHz or ...?

I suuggest to make an update event after each config of timer so the new one (prescaler, ARR...) are taken into account immediately (you can conclude from the reference manual that the timer needs update event to take into consideration the new config)

the update is done as following: TIM1->EGR |= 0x01;

Mit besten grüssen,

MCU Lüfter

georg23
Associate II
Posted on May 17, 2011 at 15:07

Hallo Lüfter,

der Einfachheit halber antworte ich mal in Deutsch (alternativ könntest Du mir mal Deine e-Mail an ''georg - at - cream-tea.de'' schicken, dann machen wir per PM weiter). Aber hier zunächst der Versuch bzw. mein Problem:

  • ich benutze das STM8 Discovery-Board. Für direkten Zugriff auf PC1 habe ich Lötbrücke SB3 umgelötet (wie im Board Manual beschrieben)
  • der STM8 läuft mit 16MHz externem Takt
  • die PWM wird an TIM2_CC2 (= PD3 = CN4, P8) generiert und an TIM1_CC1 (= PC1 = CN2, P2) zurückgelesen.
  • die PWM ist über die gesamte Dauer konstant (1kHz, 30%) und wird über ein kurzes Kabel von PD3 -> PC1 gegeben
  • die Korrektheit der erzeugten PWM habe ich mit einem Oszi kontrolliert (s. angehängtes Bild). Sie stimmt geradezu unheimlich gut...
  • bei 1kHz und 16MHz (PRE=0) erwarte ich einen Capture-Wert von 16000(=16e6/1e3) für die volle Periode bzw. 4800(=0,3*16000) für die high-Dauer
  • die erste Messung (direkt nach Start der PWM Generierung) liefert einen Wert ''in der Nähe'', konkret CC1=15945 und CC2=4744
  • alle weiteren Messungen (finden nur alle 5ms statt, siehe main loop) liefern hingegen Werte um die CC1=13900 und CC2=2690
  • wenn ich im Main-Loop das sleep_ms(5) VOR die erste Messung der PWM setze, erhalte ich auch in der ersten Messung Werte um die CC1=13900 und CC2=2690
  • wenn ich von aussen ein konstantes aber unkorreliertes(!) PWM Signal anlege, (z.B. von einem anderen Discovery Board) bekomme ich ganz andere Werte

Speziell die letzten 4 Punkte liessen sich einfach erklären, wenn TIM1 noch vor der ersten steigenden Flanke losläuft, obwohl ich dachte, ich habe ihn so konfiguriert, dass er genau das macht (TIM1_SMCR). Aber offenbar mache ich da was falsch, aber ich komme einfach nicht dahinter... :-( Anbei noch ein vereinfachtes Projekt. Die interessante Routine ist in ''hw_layer.c'' Z.124ff.

Für jedwede Hilfe bin ich dankbar und für Deine Mühe vielen Dank im voraus!

Gruss, Georg

PS: Anbei ein Screenshot der PWM sowie das Projekt
lowpowermcu
Associate II
Posted on May 17, 2011 at 15:07

Hi georg,

Entshuldigung, aber ich verstehe ein bischen Deutsch

deshalb schlage ich vor, um Ihre Nachricht auf Englisch übersetzen

.

Danke shön,

MCU Lüfter