cancel
Showing results for 
Search instead for 
Did you mean: 

Linux support

herzog
Associate
Posted on March 06, 2010 at 02:36

What a pity.

If it would support Linux, I could actually use it, now that I have mine - but it seems like Arduino is the way to go.

Another piece of good hardware wasted due to crappy software support...

2 REPLIES 2
ne562
Associate II
Posted on February 24, 2011 at 13:47

STVD works in Wine, for programming there is only one option - http://www.versaloon.com/bbs/viewtopic.php?f=2&t=17&start=0

stm2399
Associate II
Posted on March 09, 2011 at 09:11

The url (thread) andrey points to is for using (converting) the STM8S-Discovery to an ARM SWD debugger. Not to support STM8 SWIM.

I don't think that will work with the sw/port from that thread.

The Standard Versaloon dongle should support STM8 SWIM (Simon says)

/Bingo