2013-11-21 04:12 PM
I downloaded the latest STVD using the Cosmic compiler and set up a new project. When I edit a file and then try to compile it, it takes about 30 seconds to a minute to save the file before doing the compile. Makes using it almost not worth it. Any ideas on what setting could be wrong?
#stvd---cosmic-configuration2013-11-22 01:42 AM
Hello,
The delay might come from a wrong Cosmic licence handshake when launching the build. Is the build successful at the end ? Is the file saving done directly through the STVD menu (or Ctrl+S) or is the file saving automatically managed by STVD after a ''Build'' (F7) action from user ? Saving the file directly through STVD menu will show if the delay comes from the file saving action itself rather than from the ''Build'' initialization.