Hello,Have you tried to install STSW-LINK009 - ST-LINK, ST-LINK/V2, ST-LINK/V2-1, STLINK-V3 USB driver signed for Windows7, Windows8, Windows10 - STMicroelectronics ? STLINK-V3PWR descriptors have been added (especially in stlink_VCP.inf), and despit...
OK this bug will be fixed in next firmware version, which should be "P6". If you want to manage it from now on, I'm afraid you will need to implement both ways of processing depending if the "P" version is less than 6 or not [Note that I have not dec...
Hello,This raises 2 points:1. We have not validated the voltage change during acquisition because this case is not possible in CubeMonitorPwr context2. However some code is available at firmware level around this ... but is buggy: it mixes the metada...
Hello,Yes I mentioned it in my first answer. After quick review this should also affect the acknowledgment of the stop command and bypasses some consistency checks done by freq, acqtime, output and format commands; so you have to take care, in this c...
Personally I'm using putty but after checking with teraterm I have the same behavior as you. Looking at teraterm help shows that the settings signification is perhaps confusing ? For instance in receive, CR+LF means: "Received CR ($0D) character is c...