2010-01-11 01:50 PM
Is X register available for writing TIMx_CCRyH/L registers ?
2011-05-17 06:07 AM
I am investigating the usage of the PWM output. I found a code to write the TIM3_CCR2H/L registers at the TIM3_OC2Init function of the FWLib source code stm8s_tim3.c The source code behaves two 8-bit write operations for the timer registers as follows.
/* Set the Pulse value */ TIM3->CCR2H = (u8)(TIM3_Pulse >> 8); TIM3->CCR2L = (u8)(TIM3_Pulse); I assumed that the program would be more simple when the write operation is described as one 16-bit write operation like following. volatile u16 TIM3_CCR2 @ 0x00532F; : TIM3_CCR2 = (u16)TIM3_Pulse; But the program using a 16-bit variable to write the timer register has been failed, however the the line is certainly compiled into an LDW instruction sourced from X register. Why this program has been failed ? Is the WRITE operation order of the LDW instruction different from what the timer register expected ? --- noritan.org [ This message was edited by: st16 on 10-01-2010 15:34 ]2011-05-17 06:07 AM
Hi,
I think that is a security mechanism that is consist to write first the CCR2H register before the CCR1H. Regards Anis2011-05-17 06:07 AM
Hi Anis,
you're right, see reference manual pag. 161 paragraph 17.5.1 (it is for TIM1, but it's valid also for other timers). On 8-bits microcontrollers this kind of read and write mechanism protection is usual 🙂 for r/w access of 16-bit or 10-bit registers as in the case of ADC converted value. brazov :(2011-05-17 06:07 AM
Hi Anis, brazov
I assumes that the mechanism is for security reason and many other 8-bit MCU with 16-bit timer have same kind of one. It is reasonable for STM7 because STM7 has 8-bit registers only. But STM8 has 16-bit registers X and Y. I wonder why the firmware library is still using 8-bit access to the 16-bit timer registers and why STM8 will fail if access to the 16-bit register by the 16-bit X register. --- noritan.org