cancel
Showing results for 
Search instead for 
Did you mean: 

Hypoterminal is dead

Andrew Neil
Evangelist III
Posted on September 16, 2010 at 23:33

It's not even as if Hyperterminal is a standard part of Windows any more:

http://windows.microsoft.com/en-US/windows-vista/What-happened-to-HyperTerminal

5 REPLIES 5
Posted on December 20, 2016 at 05:08

I've tried to avoid it for many years.

I use RealTerm rather a lot for the hex modes, send and capture options. For things where I need file transfer capabilities I found Clear Terminal to be quite effective.

http://download.cnet.com/windows/clearconnex/3260-20_4-10097791-1.html

 
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist III
Posted on December 20, 2016 at 22:24

No, I really don't think that was a question asked by me 6 years ago!

Far more likely, this was a reply to something else which has got disconnected from its original question.

Good to see ST keeping up the quality with the new forum ...

Posted on December 21, 2016 at 16:49

And Microsoft does that very well, too... that link in the OP is rotten.

Good to see you around, Andy.

Jan

Posted on December 21, 2016 at 18:40

I replied to the old thread some what out of amusement, it came up as a 'related' topic/thread to one I had been looking at, and I was also trying to get my head around 'marking something as obsolete' which apparently not something I can do as a user.

I'd be further amused if the new forum software actually emailed you an alert about this, or if it just popped up in the InBox here..

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Andrew Neil
Evangelist III
Posted on December 21, 2016 at 20:49

Yes, it was the forum that emailed me an alert of this thread's resurrection!

0690X00000605v2QAA.png

Also:

0690X00000605rfQAA.png

Note to any potential spammers: none of the above is a real email address!