cancel
Showing results for 
Search instead for 
Did you mean: 

#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\modsl0.h:1 FlexLM No such feature

irfan karazor
Associate III

#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\modsl0.h:1 FlexLM No such feature exists.

i am using FSE_Compiler.

How can I fix this problem?

4 REPLIES 4
S.Ma
Principal

Maybe FlexLM relates to toolchain license, to renew, or the memory model used to compile is not useable.

What can i do fix it?

Do you have any offer?

irfan karazor
Associate III

Software of modslo.h is:

/* LARGE STACK MODEL <64K FOR STM8 COMPILER

 * Copyright (c) 2006 by COSMIC Software

 */

#pragma space () @near

#pragma space * () @near

#pragma space const []

#define __MODSL0__ 1

#error cpstm8 C:\Program Files (x86)\COSMIC\FSE_Compilers\CXSTM8\Hstm8\modsl0.h:1 FlexLM No such feature exists.

Franco77
Associate II

It seems to be a Cosmic license issue. Did you get the free license file from Cosmic company? When you install the free tool into a new workstation you have to communicate the PC data to the software house, they will answer with a new license file.