cancel
Showing results for 
Search instead for 
Did you mean: 

CANNOT FIND "Connect Under Reset" option in the Target -> settings menu in the STM32 ST_LINK utility. The primary problem is that i cannot connect my st_link to the utility. I have aready updated the firmware

G.M.
Associate II
 
This discussion is locked. Please start a new topic to ask your question.
6 REPLIES 6
waclawek.jan
Super User

Target->Settings, a Settings window opens:

0690X000008wGj4QAE.png

JW

G.M.
Associate II

I haven't that option on the list, i only have Normal and Hot Plug options

G.M.
Associate II

And i also can't modify the frequency in the port configuration section

Not much to work with here. Doesn't find the ST-LINK? Doesn't find the Target the ST-LINK is attaching too?

What version of the Utility? What board or ST-LINK pod involved.

0690X000008wGjJQAU.jpg

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
G.M.
Associate II

It find ST-LINK, version V1, i am using an stm8s discovery demoboard

waclawek.jan
Super User

Ah, V1 has its limitations...

But you should be able to do "connect under reset" also "manually" - hold the NRST line low, while attempting to connect. If it does not work, you have a serious problem.

Is the original target (the STM8) disconnected? Do you use a short cable to connect to the STM32 target?

JW