2009-01-19 9:56 PM
EMC design: How to set TRAP instruction on all unused flash code?
2011-05-17 6:02 AM
Dear All,
EMC design How to set TRAP instruction on all unused flash code? I want to fill unused flash memory with 0x83 (Trap instruction) How it is possible with: IDE: STVD 4.10 Compiler Cosmic 4.2.7. Thanks [ This message was edited by: cyril.rieu on 19-01-2009 17:28 ]2011-05-17 6:02 AM
look for the -f option in the linker section of the manual: I'm not sure if STVD allows to manage this via the graphical interface, but, worst case, you can edit the .lkf file by hand.
Regards, Luca (Cosmic)2011-05-17 6:02 AM
thanks _luca.
Solution: it is possible to set this option in Project->settings->[tab]Linker Category ''input'' at the end of the section name if -m set. and add -f0x83 (filling with trap opcode) We obtain this line in lkf file +seg .const -b 0x8f00 -m 0xf100 -n .const -it -f0x83