2024-08-22 12:46 PM
Join us for an exciting workshop featuring ST’s STM32 NUCLEO-H7S3L8 development board — yours to keep! This three-hour interactive session offers personalize instruction, engaging discussions, and practical hands-on exercises to familiarize you with the new STM32H7R and STM32H7S microcontrollers, ST’s fastest MCUs equipped with a Cortex-M7 CPU core running at 600MHz. Discover how these cost-effective “boot-flash” MCUs will enhance your projects.
STM32H7R and STM32H7S microcontrollers embed a 2.5D NeoChrom GPU for the development of sophisticated GUIs that can operate smoothly at 60FPS with WXGA resolution. This makes it possible to run MPU-like applications on an economical real-time MCU. Furthermore, all H7 models comply with the strict security requirements of SESIP Level 3 and PSA Level 3 certifications, offering physical attack protection and advanced encryption mechanisms for external flash and RAM modules.
Register here: https://resources.embeddedcomputing.com/Embedded-Computing-Design/STM32H7RS-MCU?utm_bmcr_source=PH
2024-08-22 11:48 PM
Is the hands-on at Embedded world Austin?
2024-08-23 3:24 AM
Yes it is live during embedded world North America.