2009-12-04 12:58 AM
default location vectorjump.o using auto linker
2011-05-17 6:06 AM
Hi,
(second attempt. For some reason the text disappeared when i send the forum post.) I need to redirect the interrupt vector table from 0x8000 to 0xA880 to get the custom bootloader working. With the help of the ST forum I found out how to redirect the interrupt vector table. With the following command in the linker file I can place the code (vectorjump.o) below at location 0x8000. +seg .const -b 0x8000 -k Debug\vectorjump.o #include ''main.h'' struct interrupt_vector { u32 interrupt_instruction; }; struct interrupt_vector const _jumptab[] = { {START_CBL_INTERRUPT_VECTORS}, /* RESET */ {(START_INTERRUPT_VECTORS + 4)}, /* TRAP - Software interrupt */ {(START_INTERRUPT_VECTORS + 8)}, {(START_INTERRUPT_VECTORS + 12)}, {(START_INTERRUPT_VECTORS + 16)}, {(START_INTERRUPT_VECTORS + 20)}, {(START_INTERRUPT_VECTORS + 24)}, {(START_INTERRUPT_VECTORS + 28)}, {(START_INTERRUPT_VECTORS + 32)}, {(START_INTERRUPT_VECTORS + 36)}, {(START_INTERRUPT_VECTORS + 40)}, {(START_INTERRUPT_VECTORS + 44)}, {(START_INTERRUPT_VECTORS + 48)}, {(START_INTERRUPT_VECTORS + 52)}, {(START_INTERRUPT_VECTORS + 56)}, {(START_INTERRUPT_VECTORS + 60)}, {(START_INTERRUPT_VECTORS + 64)}, {(START_INTERRUPT_VECTORS + 68)}, {(START_INTERRUPT_VECTORS + 72)}, {(START_INTERRUPT_VECTORS + 76)}, {(START_INTERRUPT_VECTORS + 80)}, {(START_INTERRUPT_VECTORS + 84)}, {(START_INTERRUPT_VECTORS + 88)}, {(START_INTERRUPT_VECTORS + 92)}, {(START_INTERRUPT_VECTORS + 96)}, {(START_INTERRUPT_VECTORS + 100)}, {(START_INTERRUPT_VECTORS + 104)}, {(START_INTERRUPT_VECTORS + 108)}, {(START_INTERRUPT_VECTORS + 112)}, {(START_INTERRUPT_VECTORS + 116)}, {(START_INTERRUPT_VECTORS + 120)}, {(START_INTERRUPT_VECTORS + 124)}, }; To do this I need to alter manually the linker file. Before this I always used the auto linker option Project->settings-.linker->input-> auto Is there a way to get the same result but with the auto linker? [ This message was edited by: r.hoek on 08-12-2009 14:23 ]2011-05-17 6:06 AM
Hi Hoek,
Please add more details