Posted on May 17, 2011 at 15:06Hi, (second attempt. For some reason the text disappeared when i send the forum post.) I need to redirect the interrupt vector table from 0x8000 to 0xA880 to get the custom bootloader working. With the help of the ST f...
Posted on May 17, 2011 at 15:05nevermind the questings in de last reply, I got it working now. make a few mistacs: Firmware starting locations I needed to alter the starting address of the firmware (0x8080) and its interrupt table (0x8000). that is ...
Posted on May 17, 2011 at 15:05Hi, I am working on a custom bootloader code for the STM8S207 / 208. for 90% its finished, I can write the firmware to flash with my custom bootloader. also reading, erassing and other things. the next step is to jump ...