2009-10-02 12:13 AM
Control the initial level while using the Timer output compare mode
2011-05-17 6:04 AM
Hi,
I'm using the Timer 3 in output compare mode with toggles, each time the interrupt occurred, I have to change the next match value (TIMx->CCRn). My question is: is it possible to set the initial state in a known level? I'vd try to use GPIOx->ODR, but this seems not work.2011-05-17 6:04 AM
Hi,
You can configure the mode PWM mode1 or PWM mode2 in the TIMx_CCMR1 register and then select the polarity (CC1P bit) in the TIMx_CCER1 Capture/compare enable register 1. regards mozra