2016-03-21 2:40 AM
Hello!
I compile sourse code stvp (http://www.st.com/web/en/catalog/tools/PF257522) in visual studio 2015.The program displays
an error
in console: >>> Programming PROGRAM MEMORY (API) ERROR : Cannot communicate with the tool. Wrong tool selection or check tool power supply or check that a previous session is closed. <<< Programming PROGRAM MEMORY failsFull log: D:\workspace\ApiSample\Debug>APISample.exe -Device=STM8S103K3 -ProgMode=SWIM -Port=USM -FileProg=D:\ELload.hex STVP_CmdLine version 1.4 Verbose ON Log activity ON Display Progress OFF Message box warning if protect option byte ON Loop mode ON Erase device OFF Blank check device OFF Verify device ON Configuration: BoardName=ST-LINK Device=STM8S103K3 Port=USM ProgMode=SWIM >>> Filling PROGRAM MEMORY image in computer with Blank Value <<< Filling PROGRAM MEMORY image in computer succeeds >>> Loading file D:\STProjectGIT\El_load_2\Release\Exe\ELload.hex in PROGRAM MEM ORY image in computer <<< Loading file succeeds >>> Programming PROGRAM MEMORY (API) ERROR : Cannot communicate with the tool. Wrong tool selection or check tool power supply or check that a previous session is closed. <<< Programming PROGRAM MEMORY fails #stvp #stm8 #st-link2016-03-21 6:20 AM
Hello,
Check your syntax, the port is USB, not USM. You can also use the STVP_CmdLine.exe installed with the toolset in STVP directory. Rgds, Laurent2016-03-21 8:03 AM
stvp has been installed. I write ''USB'', but nothing change.
2016-03-21 8:49 AM
Is it an ST board (discovery) ?
If not, did you check connections ? What is the OS used ? Can you see the STLink (USB) in device manager ? Does STVP connect to the STLink and STM8 target without issues ? Can you try with the STVP_CmdLine.exe installed in STVP. Rgds, Laurent2016-03-21 9:53 AM
I use ST-LINK. STVP_CmdLine.exe is works,
but
the compiled
application in vs2015
(http://www.st.com/web/en/catalog/tools/PF257522) does not work.2016-12-12 5:36 AM
I also have the problem.
I downloaded the program, registered and then installed it.
This error message then comes ''Cannot communicate with the tool.
Wrong tool selection or check tool power supply or check that a previous session is closed.''.USB has detected the PC and I can not go any further.
From Result.log:
new log session
date: 12/12/16time: 13:59:59----------------------------------------------------------STVP_CmdLine version 1.6NO ARGUMENTS GIVEN: will use default config. Type STVP_CmdLine -help for usage
Configuration:
BoardName=ST-LINK Device=STM8L15xC6 Port=USB ProgMode=SWIMProgMemFileName=ProgMem.hexOptionFileName=Option.hexVerbose ON
Log activity ONDisplay Progress OFFMessage box warning if protect option byte ONLoop mode ONErase device OFFBlank check device OFFVerify device ON>>> Filling PROGRAM MEMORY image in computer with Blank Value<<< Filling PROGRAM MEMORY image in computer succeeds>>> Loading file ProgMem.hex in PROGRAM MEMORY image in computer
<<< Loading file succeeds>>> Loading file Option.hex in OPTION BYTE image in computer
<<< Loading file succeeds>>> Programming PROGRAM MEMORY
Cannot communicate with the tool.Wrong tool selection or check tool power supply or check that a previous session is closed.<<< Programming PROGRAM MEMORY fails2017-01-05 11:45 PM
Hello, I'm back again.
With the STM8-Discovery the connection has now folded.
I have connected the ST-Link / V2 and this has automatically installed the driver.Then I connected the STM8-Discovery and lo and behold, it worked.
Thanks for your feedback!