cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupt not working

ST MICROCONTOLLER
Associate II
Posted on December 21, 2016 at 13:02

I am trying to run a code in which timer causes an interrupt and everytime interrupt is generated, a variable h is incremented, but it remains zero in quickwatch window. My code is written below in stvd and cosmic compiler.

#include 'stm8s.h'

#include 'stm8s_tim1.h'

#include 'stm8s_itc.h'

#define TIM1_PSCRH (*(volatile uint8_t *)0x5260)

#define TIM1_CR1    (*(volatile uint8_t *)0x5250)

#define TIM1_ARRH    (*(volatile uint8_t *)0x5263)

#define TIM1_ARRL    (*(volatile uint8_t *)0x5264)

#define TIM1_PSCRL    (*(volatile uint8_t *)0x5261)

#define TIM1_IER (*(volatile uint8_t *)0x5254)

int h;

void main(void)

{

            //TIM1_SetCounter(5);enableInterrupts();GPIO_Config();

            //TIM1_DeInit();

TIM1_ARRH=0X55;

TIM1_ARRL=0X26;

TIM1_PSCRH = 0x3e;

TIM1_PSCRL = 0x80;

TIM1_CR1=0X81;

TIM1_IER=0X01;

enableInterrupts();

      while(1)

      {

        

       }

         }

INTERRUPT_HANDLER (TIM1_UPD_OVF_IRQHANDLER,23)

//@interrupt @far void TIM1_OVF_TRG_BRK_IRQ_Handler(void)

{

    h++;

}

    

#ifdef USE_FULL_ASSERT

/**

  * @brief  Reports the name of the source file and the source line number

  *   where the assert_param error has occurred.

  * @param file: pointer to the source file name

  * @param line: assert_param error line source number

  * @retval None

  */

void assert_failed(uint8_t* file, uint32_t line)

{

  /* User can add his own implementation to report the file name and line number,

     ex: printf('Wrong parameters value: file %s on line %d\r\n', file, line) */

  /* Infinite loop */

  while (1)

  {

  }

}

#endif

What is wrong with the code? Kindly help me.

Thank you.

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
Schmidt.Andreas
Associate II
Posted on December 21, 2016 at 15:48

Hi,

try to use : volatile int h;

Regards

Andreas

Seb
ST Employee
Posted on December 21, 2016 at 16:28

Are you using the debugger? 

Is the code enabling timer internal clock so you can actually write the timer registers?

In an old code, I've got this:

  CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE);

Put as first step... (STM8L151)

==============================

Digging at the std lib:

void CLK_PeripheralClockConfig(CLK_Peripheral_TypeDef CLK_Peripheral, FunctionalState NewState)

{

/* Check the parameters */

assert_param(IS_CLK_PERIPHERAL(CLK_Peripheral));

assert_param(IS_FUNCTIONAL_STATE(NewState));

if (((uint8_t)CLK_Peripheral & (uint8_t)0x10) == 0x00)

{

if (NewState != DISABLE)

{

/* Enable the peripheral Clock */

CLK->PCKENR1 |= (uint8_t)((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F));

}

else

{

/* Disable the peripheral Clock */

CLK->PCKENR1 &= (uint8_t)(~(uint8_t)(((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F))));

}

}

else

{

if (NewState != DISABLE)

{

/* Enable the peripheral Clock */

CLK->PCKENR2 |= (uint8_t)((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F));

}

else

{

/* Disable the peripheral Clock */

CLK->PCKENR2 &= (uint8_t)(~(uint8_t)(((uint8_t)1 << ((uint8_t)CLK_Peripheral & (uint8_t)0x0F))));

}

}

}

and yes, you need to declare the variable as volatile to be sure.

simon ferrer
Associate II
Posted on December 21, 2016 at 23:08

Have you enabled the interrupt at NVIC Level?

Posted on December 22, 2016 at 07:10

Thanks, but declaring variable h as volatile didn't make any change.

Posted on December 22, 2016 at 07:13

Thanks, I am using stm8s003k3 board with debugger, but the value of h is seen as 0 in simulator also.

Posted on December 22, 2016 at 07:15

Thanks, do I have to edit any of the header files to enable interrupt at NVIC level?

Posted on December 22, 2016 at 07:21

Also, putting line

  CLK_PeripheralClockConfig(CLK_Peripheral_TIM1, ENABLE);

resulted in error 'redeclared external CLK_PeripheralClockConfig'

Posted on December 22, 2016 at 11:23

This type of error seems to tell the source code has an issue like missing/too many ) or }

Calling a function should not yield such error.

ST MICROCONTOLLER
Associate II
Posted on December 22, 2016 at 14:23

I have included stm8s_itc.h. I have seen somewhere stm8s_it.h file being included, which I think, is supported for raisonance as well as cosmic. When I include that file, another error takes place  'symbol f_NonHandeledInterrupt multiply defined'

Thank you.