STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM8L101 clocking at < 2 MHz

Posted on October 15, 2015 at 15:12Hello All, Is there any way to run STM8L101 at a frequency about 200 kHz to save some microAmps?BR, Dmitry #frequency #stm8l101

Dmitry A by Associate
  • 839 Views
  • 2 replies
  • 0 kudos

STVD Toolset configuration for STM8 Cosmic

Posted on October 19, 2015 at 21:45Hello, We are planning to start to use STM8 automotive microcontroller in one of our product. To start with we downloaded STVD development suite (C:\Program Files (x86)\STMicroelectronics\st_toolset) and Cosmic (C:...

suresh by Associate II
  • 1273 Views
  • 2 replies
  • 0 kudos

STVD Toolset configuration for STM8 Cosmik

Posted on October 19, 2015 at 21:40Hello, We are planning to start to use STM8 automotive microcontroller in one of our product. To start with we downloaded STVD development suite (C:\Program Files (x86)\STMicroelectronics\st_toolset) and Cosmic (C:...

suresh by Associate II
  • 692 Views
  • 0 replies
  • 0 kudos

PROBLEM WITH IAR AND UNI/O

Posted on October 14, 2015 at 16:16Good afternoon, I have a problem, our STM8L uC should communicate with an EEprom 11LC by Microchip  using the UNI/O bus. When we send the data however the EEPROM do not answer. We are programming using IAR Someone ...

LIN Protocol STM8AF/AL

Posted on October 14, 2015 at 07:07Hello All,I am new to LIN and started working on it While creating the LIN PID/Identifier can we give our own ID number or is there any constraints , if yes what are the constraints.Thanks in advance.  #lin-prot...

Need program to count the number of times the user button pressed and according to count i should change the further task

Posted on October 07, 2015 at 07:19Hello All,I am a beginner in STM8 bit controllers.Currently using STM8AF board.In this i need to count the number of times that i press the userbutton1/userbutton2 and according to the count i should perform some s...

Hi All, what compiler should i use?

Posted on August 17, 2010 at 04:07 Hi All, what compiler should i use? #stm8-compilers #compiler #raisonance #cosmic #iar

leoren_tm by Associate II
  • 4965 Views
  • 13 replies
  • 0 kudos

Check RAM

Posted on October 02, 2015 at 03:54Dear All.In STM8S have 1k RAM. So I want to check all RAM before use this. The first i will write data on RAM and then Read  and compare. But i don't know how to define address of RAM.Example: I want to write value...

cv-chung by Associate
  • 666 Views
  • 0 replies
  • 0 kudos

stm8s discovery version

Posted on March 28, 2015 at 17:19Hi guys, I am developing the lypus tool(a stm8 tool for Linux) for what I know stm8s discovery has a stlinkv1 in a STM32F103C8T6?! Does stlinkv1 is the unique version in the stm8 discovery boards range? can we update...

lmx1 by Associate II
  • 826 Views
  • 2 replies
  • 0 kudos

Super-basic questions

Posted on October 01, 2015 at 17:02In need of help... I have been given a .s19 program that I need to load onto a STM8F board. I don't need the L board. I have absolutely 0 experience with this programming environment, and am having trouble finding ...