STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

External timer trigger on STM8S003_F_?

Posted on November 20, 2015 at 10:00Hi!I have to generate a PWM that must  be quite closely synced to an external signal of 50 Hz (to avoid any drifts).From the documentation contents of STM8S008F/K of it using the TIM1 external trigger (ETR) to res...

Cosmic compiler Error

Posted on November 18, 2015 at 12:34Thank you Luca,   As per your reply we already change the workspace toolset Rootpath as follows:      ''C:\Program Files\COSMIC\32K_Compilers\CXSTM8''but I can't understand the meaning of- your linker file specifi...

Stm8 TSL and double touch

Posted on December 17, 2013 at 14:31Hello everyone. I am making Kitchen Clock on STM8S105C6 and STM8 touch sence library. I need 4 buttons and  i have configurate them as SCKEY. Now they works fine. My problem is that library catch only one button a...

COSMIC compile error

Posted on October 13, 2015 at 16:41When I go to compile the sample code from ST's site, I get the error ''Can't Access File: .Idea_Temp\IDEABLD.BAT in Project directory. Check access rights .....'' I tried searching for IDEABLD.BAT, and I can't find...

jherrmann by Associate II
  • 1426 Views
  • 2 replies
  • 0 kudos

Swim - Chip does not answer

Posted on September 06, 2012 at 09:37Hi, I am debugging software for an STM8S105x6, using the programmer from the STM8S-Discovery board and STVD software. All went fine, until suddenly an error popped up while entering debug mode: '** Connection err...

STLUX (STM8) Storing interrupt vector table in RAM.

Posted on November 10, 2015 at 14:56 Hi All, I am during writing bootloader for STLUX processor (base on STM8). Both, bootloader and main program uses own interrupt vector table. The STM8 processor has fixed interrupt vector table at 0x8000 ...

0690X00000602o2QAA.jpg

RAM value when statup and reset

Posted on November 03, 2015 at 03:05Dear All,When STM8 power on or after reset, how about value of RAM  (0x00 or 0xff or another value).I try to search on the internet about RAM structure of STM8 but don't have any documentThanks.

cv-chung by Associate
  • 632 Views
  • 0 replies
  • 0 kudos

Uart Receive is not working

Posted on October 29, 2015 at 10:00 I am new to STM I have written following code in iar but couldn't able to receive from uart. // // This program shows how you can output a message on the UART on // the STM8S microcontroller. // // T...

[HELP]Can we create delay 1 microsecond with TIMER4?

Posted on November 01, 2015 at 16:00Hello everyone, I am using STM8S105 and STM8S003. Can we create delay 1 microsecond with TIMER4? I can create delay 1ms, 100us, 10us but can not for delay 1us. Can we? Thank you!

How to use standard peripheral library for stm8s003f3p

Posted on October 29, 2015 at 10:08I am working on STM8S3F3P , when i tried to standard peripheral for this microcontroller i keep getting error that select predetermined chip from STM/A.Is there any tutorial to learn this..