STM8 MCUs

Discuss STM8 microcontrollers, including SWIM, USART configurations, RTC usage, ADC issues, and debugging.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STVD workspace location limitation?

I wish to use STVD to set up a new workspace on a mapped common drive but it whereas I can see and go to a mapped drive with the Atmel IDE etc the STVD IDE doesnt appear to recognise it. Is this a known limitation or something I am doing wrong?

BCowa by Associate II
  • 502 Views
  • 0 replies
  • 0 kudos

How to get interrupts work when compiling from command-line?

I set up a project that generates the makefiles for the STM8 target. It almost works, just the interrupt vector table is not updated with the definitions in the code.The interrupts are set up and work. I can see that from the button press on the disc...

GANG PROGRAMMER FOR STM8S

For the mass production i am want gang programmer or I need to program through UART without any bootl-oader firmware.

NM by Associate III
  • 562 Views
  • 0 replies
  • 0 kudos

stm8s105k4 CCO does not output

here is the code https://gist.github.com/goog/222020c4d46e751f591559f3f3ff06e0BUT the PD0 does not output clockI'm new to stm8 and reference STM8S_StdPeriph_Lib example

Resolved! Sample USART project for STM8L-Discovery

I have a big problem when using USART on STM8L-DISCOVERY. I studied the reference manual but it didn’t help me. I use library SPI. Could you send me a project working with usart on STM8L-DISCOVERY please!!!! NOTE: This question and answer originated ...

How to expand array size in memory(Error- segment .bss overflow)?

Hi there,I want to expand array size until 3000. (i.e. arr[3000]). I have 4KB RAM.currently I can get value till arr[1500].I tried different options to expand size but no success. Please see below image.How to expand array size? Thanks ,Gopal

0690X000009YqyfQAC.png
Gopal by Associate
  • 671 Views
  • 1 replies
  • 0 kudos

STM8S003 program disappears

I am currently using STM8S003 and use to option byteDuring normal use, sometimes the program suddenly disappears.Then when re-burn, it will fail and the following message will show:Errors while setting configuration with MCU name STM8S103F3P: gdi-err...

LYang.3 by Associate
  • 490 Views
  • 0 replies
  • 0 kudos