I have been using ST Visual Developer version 4.3.12 for weeks. Today it started crashing when I begin a debug session. I am running Windows 7 Ultimate. There was a system update for Windows Defender completed today (Definition 1/295.207.0) as wel...
I have a legacy design with a STM8L052C6 MCU. There is a 4x3 matrix keypad. I am trying to drive the Rows and scan the columns. The C1 port only rises to about 0.5V when I set the pin HIGH. Is there something I am missing.There are three ports set a...
Turns out that the issue was not the code nor the MCU; the issue was that the scope digital pod I was using presented a 100K load on the MCU pins and that was enough to overload the drive capability and cause the pin's reduce signal and stop the rece...