cancel
Showing results for 
Search instead for 
Did you mean: 

Any tips to solve this APPCRASH ntdll.dll error?

RhSilicon
Lead

Hello,

Problem opening the Programmer, I can't click on the Integrated Circuit icon.

The error occurs almost always, eventually when reinstalling, once or twice the programmer window opens correctly. After giving this error, it does not open again and only presents an error.

The problem occurs even in a newly installed system, 32 or 64 bits.

Tested with Windows 7 and Windows XP, which System should work?

Since 2017 there are no updates. Any possibility of making a plugin for Eclipse?

The SDCC compiler already supports STM8S, and it works on Linux as well.

0693W00000bhCskQAE.png

1 REPLY 1