cancel
Showing results for 
Search instead for 
Did you mean: 

stm32mp157FAD ,the MPU restarts when U-Boot run to boot over usb0 . this happens again and again

xingya
Associate

cubeProgram.jpgterminal.jpg

U-Boot 2020.01-stm32mp-r1 (Oct 07 2023 - 14:05:57 +0800)

CPU: STM32MP157FAD Rev.Z
Model: STMicroelectronics STM32MP157F eval daughter
Board: stm32mp1 in trusted mode (st,stm32mp157f-ed1)
DRAM: 512 MiB
Clocks:
- MPU : 800 MHz
- MCU : 208.878 MHz
- AXI : 266.500 MHz
- PER : 24 MHz
- DDR : 533 MHz
WDT: Started with servicing (32s timeout)
NAND: 0 MiB
MMC: STM32 SD/MMC: 1
In: serial
Out: serial
Err: serial
invalid MAC address in OTP 00:00:00:00:00:00
Net:
Error: ethernet@5800a000 address not set.
No ethernet found.

Hit any key to stop autoboot: 0
Boot over usb0!

 

==================

When the program runs here, the MPU restarts, and this happens again and again

 

0 REPLIES 0